alert icon

Internet Explorer 8 or 9 is not supported by this website. Please either update your version of Internet Explorer, or use a more up to date browser.

Hide Message hide icon
San Diego | Orange Fluid System Technologies

Your Authorized Swagelok Product and Service Center

2019 Product Changes

Notification of Change Level 1

Swagelok has earned a reputation for unmatched quality and consistency at the component level. We are committed to maintaining this reputation while continuing to grow and improve our product offering. At times, this requires changes to the form, fit or function of our core products.

This Level 1 - Notification of Change sets forth changes to one or more of the products you may have purchased from Swagelok or an authorized Swagelok sales and service center. Prior to release, each change listed was carefully evaluated in accordance with the Swagelok Quality System, to minimize impact to you, our end customer. 

A Level 1 Notification relates to an applicable* change impacting Form, Fit and/or Function ("FFF") or the cosmetic appearance of a standard product. "Standard product" is any product that does not include a customer specified product or process attribute and can be purchased by any customer. This includes off-catalog product that can be assembled through designators, assemble to order ("ATO"), make to order ("MTO"), product produced by other means.

Unless otherwise noted, all changes are rolling changes and will take some time to flow through our global inventory. If you have questions regarding the impact of this change on your applications, please contact your local authorized Swagelok sales and service center representative. They, along with regional technology centers, and trained field engineers, are available to assist you.

The Following Level 1 Changes have been communicated:   

 

Effective Date: November 26, 2019
Product Name: Snoop® Liquid Leak Detector Fill Level

Description and Reason for Change: Historically, the 2 ounce, 8 ounce, and gallon size bottles of Snoop and Real Cool Snoop were inadvertently overfilled. Effective immediately the fill volume is being adjusted to reflect the listed amount. Please be assured that the that the proper fluid amount is being provided. Reference the image for an example.

In addition, the caps on gallon size containers will transition from a standard cap to a safety cap over the next three to four months. This will prevent caps from accidentally coming loose. This will be a running change so you may receive orders with both cap styles until stock of the old style is depleted.


Effective Date: December 1, 2019
Product Name: T Series PTFE Hose
Description and Reason for Change: 
Swagelok's Hose Service Group is pleased to announce that the T Series PTFE hose will be transitioning from a swaged to a crimped design for assembly of end connections starting December 1, 2019. 

While this change will allow us to increase manufacturing efficiency, we also anticipate these advantages:

  • Improved product performance allowing for increased pressure ratings at elevated temperatures that will be updated, along with the product dimensions, in the Hose and Flexible Tubing catalog.
  • Inclusion into local distributor crimp cell capabilities for local assembly.

The current swaged design will continue to be the only version supplied until December 1, 2019. Following that date, crimped ends will be supplied as end connection inventory of swaged assemblies are depleted. You may see both designs in orders containing multiple end connection types until the transition is complete.


Effective Date: August 30, 2019
Product Name: PB Series Rubber Hose
Description and Reason for Change: 
As a part of our effort to provide exceptional service to our customers and to facilitate ideal packaging of PB series hose and end connections, there is a change to the product line. Swagelok is making a design improvement on the end connections that will eliminate the finishing cap. This change will allow for bulk packaging, eliminating the need to cut open individual bags, and provide a cleaner visual appearance.

The removal of the finishing cap may require minor changes to the length and/or outside dimension of the end connection. An updated Hose and Flexible Tubing catalog is available and reflects the dimensional changes associated with the new end connection, as well as the visual changes due to the removal of the finishing cap.

The new supply of bulk hose may have minor visual differences specific to the color and surface finish. The same color options will be provided, however, there may be slight differences in the shade of the colors. The gray color hose will contain black text in place of white text. The black color bulk hose will be constructed with a Neoprene cover for added UV and ozone resistance. The hose reel size and/or material may also change.


Effective Date: September 30, 2019

Product Name: Swagelok Facing Tool Service Update for SWS-232EP Model

Description and Reason for Change: 

Swagelok will no longer service the SWS-232EP model facing tool as of September 30, 2019, or until spare parts can no longer be supplied, whichever comes first.  Sales of the SWS-232EP were discontinued in 2011 in conjunction with the release of the MS-TF series facing tools.

Swagelok continues to offer the MS-TF series facing tools. Refer to Tube Facing Tools, TF16, TF24, TF40, and TF72 Series, MS-02-426, for additional information on those models. We have continued service and support of the SWS-232EP facing tool since 2011. However, our suppliers are no longer able to supply components to meet our servicing commitments for the SWS-232EP.


Effective Date: July 1, 2019
Product Name: PB Series Rubber Hose End Connections
Description and Reason for Change:

As a part of our effort to provide exceptional service to our customers and to facilitate the packaging of PB series hose and end connections, two changes are being made to the product line. First, Swagelok is making a design improvement on the end connections that will eliminate the finishing cap. This change will allow for bulk packaging, eliminating the need to cut open individual bags by you or your customer, and provide a cleaner visual appearance. Second, we are moving the bulk hose product to a new supplier. The new supplier is already used for other Swagelok products.

Product ratings will be unchanged as the new supplier will meet the same performance requirements. Swagelok has validated both bulk hose suppliers for both end connection designs to ensure there is no concern for intermix between designs or suppliers. These changes will go into effect no earlier than July 1st, 2019. Following that date, there will be a transition period where both end connection designs may be received in orders as existing inventory is depleted. 


Effective Date: January 9, 2019

Product Name: FKB Series Medium-Pressure Ball Valve Standard Handle 
Description and Reason for Change: 

Swagelok is continuously looking for ways to improve our products. The standard handle for the FKB series ball valve has been changed to incorporate a blue vinyl sleeve for increased gripping power, replacing the blue powder coating. These changes will improve functionality and simplify the standard product offering. The new handle is non-positionable. The positionable handle is available as an option. 


Effective Date: February 2019
Product Name: 
Crimping for Thermoplastic Hose Assemblies
Description and Reason for Change:

As part of ongoing continuous improvement efforts, our assembly process for TP hose will be standardized to use only crimping, effective February 1, 2019. This was one of several opportunities for enhancing hose assemblies identified through hose assessments in 2017 and 2018. The standardization will promote assembly consistency, optimize implementation of best practices, and streamline service and support for crimp tooling and equipment.

We will continue to support customer swaging of thermoplastic hose through the availability of swaging equipment and components


Review 2018 Change notifications

Review Pre-2018 Change notifications

* Applicable changes which would require notification to a Distributor or end user include changes which impact the form, fit or function of a product attribute or measurement as described in Swagelok data readily available to customers or when a change is made that is cosmetically detectable to the customer.


Effective Date: 6/1/17

Product Name: Snoop Liquid Leak Detector

Description and Reason for Change: 

The design for the 2 ounce Snoop bottle has been changed to provide improved seal integrity and an appearance aligned with the 8 ounce bottle, updated in 2016. The plug, tube, and cap will all be the same components used with the 8 ounce bottle. Old style bottles will be used until stock is depleted. The packaging will change accordingly to accommodate the new footprint of the bottle.


Effective Date: 6/1/17

Product Name: Snoop Liquid Leak Detector

Description and Reason for Change: 

The design for the 2 ounce Snoop bottle has been changed to provide improved seal integrity and an appearance aligned with the 8 ounce bottle, updated in 2016. The plug, tube, and cap will all be the same components used with the 8 ounce bottle. Old style bottles will be used until stock is depleted. The packaging will change accordingly to accommodate the new footprint of the bottle.