Product Changes
Notification of Change Level 1
Swagelok has earned a reputation for unmatched quality and consistency at the component level. We are committed to maintaining this reputation while continuing to grow and improve our product offering. At times, this requires changes to the form, fit or function of our core products.
This Level 1 - Notification of Change sets forth changes to one or more of the products you may have purchased from Swagelok or an authorized Swagelok sales and service center. Prior to release, each change listed was carefully evaluated in accordance with the Swagelok Quality System, to minimize impact to you, our end customer.
A Level 1 Notification relates to an applicable* change impacting Form, Fit and/or Function ("FFF") or the cosmetic appearance of a standard product. "Standard product" is any product that does not include a customer specified product or process attribute and can be purchased by any customer. This includes off-catalog product that can be assembled through designators, assemble to order ("ATO"), make to order ("MTO"), product produced by other means.
Unless otherwise noted, all changes are rolling changes and will take some time to flow through our global inventory. If you have questions regarding the impact of this change on your applications, please contact your local authorized Swagelok sales and service center representative. They, along with regional technology centers, and trained field engineers, are available to assist you.
The Following Level 1 Changes have been communicated:
Effective Date: January 5, 2021
Product Name: AFS and 40 Series Valves
Description and Reason for Change: In the spirit of continuous improvement, we are changing the nylon handles used on our standard AFS and 45 series ball valves by replacing the current brass handle insert with a more robust, stainless steel handle insert. The new handle will be easier to actuate and will incorporate the handle stop into the handle, removing the need for an additional handle stop insert.
This change will not affect the handle function or any valve ordering numbers. However, it will result in a change to the size of the handle used for 45 series valves and in handle kit ordering numbers. The new handle will carry the same dimensions as the current AFS series handle.
Made-to-stock valve orders may see the old handles until stock is depleted. If you require a 45 series valve with the old handle using the brass insert, we will continue to offer kits with the old handle (ordering number BZ-5K-45-BK) for up to two years. If a customer requires a valve assembled with the original 45 series handle, the local sales and service center must contact Swagelok Technical Service.
We are implementing the same change to existing 42, 43, and 44 series handles in Q2 2021, updating the handle insert from brass to stainless steel. This will make the handle consistent with the 40G handle design, which already includes the stainless steel insert. This will not change the fit or function of these valves, and there will not be any changes to end item or handle kit ordering numbers. The transition will be implemented as inventory is depleted and you may see shipments containing both handle types during this time.
Effective Date: November 17, 2020
Product Name: 43T Series Valve Packing Material
Description and Reason for Change: As part of Swagelok's ongoing commitment to implement continuous quality improvements to meet the performance needs of demanding applications, the upper and lower packing of the 43T series ball valve is changing from PFA to Modified PTFE/D1710 type 1, Grade 1, Class B material (TFM). The TFM material is the same material currently used in the 43G valve.
This change impacts the 2-way, 3-way, angle pattern, 4-way, and 5-way configurations of the 43T series ball valve only. The 43T series 6-way and 7-way configurations as well as 41, 42, 44, and 45 series valves are not impacted by this change at this time but may be evaluated for this change in the future. There will be no impact to valve fit/function, pressure/temperature ratings, or certifications. Valve ordering numbers will remain the same.
The implementation for this new packing will be a running change. As inventory of the PFA material is depleted, valve assemblies will transition to the new TFM material. Based on current inventory, the change in material will occur within approximately 6 months.
Until this transition is complete, it is possible that customers could receive valve orders assembled with either the PFA or the TFM material. Controls will be put into place to ensure there is no mixing of packing material within the same valve.
Effective Date: November 4, 2020
Product Name: BN Series Pneumatically Actuated Bellows Valve Stem
Description and Reason for Change: In the spirit of continuous improvement, we are implementing a change to all pneumatically actuated BN series valve stems. The upper part of the stem shank will now be thicker, improving our customers' ability to consistently install the retaining ring into the proper groove on the stem.
This change does not impact the function of the valve and will only be visually detectable during maintenance of the valve. This will begin in the next 30 days. During the transition, you may see shipments of assembled valves and maintenance kits containing both versions of the stem until the existing stock is depleted.
Product Name: CW Series Aflas® Bonded Poppets
Description and Reason for Change: Small visual and chemical changes will be made to the Aflas® bonded poppet for the CW series check valve. These changes will enable Swagelok to secure long-term availability of the Aflas bonded poppet component. The visual changes are as follows and will be visible when looking though the inlet port:
- Aflas color will change from dark brown to black (ASTM D2000 material remains the same)
- A molding cavity number will be added under the “AF” material designator
None of these changes will impact the function of the product.
Product Name: 5 and 6 Series Actuators
Description and Reason for Change: In the spirit of continuous improvement and quality, we are implementing a change to all 5 and 6 series actuators by adding a bellows valve option, improving the thread engagement on the panel mount nut.
Currently, there is no counter-bore on the actuator base plate. Moving forward, all 5 and 6 series actuators will include a small counter-bore which will provide more space for the panel nut threads to engage. Please note this does not impact the function of the product.
During the transition over the next 30 days, both versions of the actuator will be shipped until the existing stock is depleted. Please note that all existing product without the counter-bore still meets Swagelok quality standards.
Effective Date: September 17, 2020
Product Name: Gaugeable Preswage Tool
Description and Reason for Change: The gaugeable preswage tool is moving from a one-piece body design to a two-piece design except for the 5/8 inch size, similar to the standard Swagelok preswage tool design. The new design uses a machined insert that is pressed into a cast body. This will result in an improvement in manufacturing output.
All functional dimensions are remaining the same. However, there will be a visual and physical difference for the tool (greater overall length and body diameter). There is no impact to product function. Ordering numbers will remain the same. Implementation for the change has begun and shipments of the new design will take place throughout October; we will be fully transitioned for the impacted sizes by the end of October.
Effective Date: August 14, 2020
Product Name: HK Series Bellows Valve Discontinuance
Description and Reason for Change: HK series brass and alloy 400 bellows valves will no longer be available after remaining inventory has been depleted. The raw material used in the production of the bellows has been discontinued and a new, robust supply chain is unavailable. The decision has been made to discontinue the product line as viable alternative products are available as listed below.
New requests will be fulfilled on a first-come, first-served basis until inventory is depleted. For applications requiring compact brass bellows valves, the brass BK series continues to be available. The H series stainless steel bellows valve will also remain available.
Please reference Bellows-Sealed Valves, H and HK Series, MS-01-36, for additional information on the H and HK series valves.
Effective Date: October 1, 2020
Product Name: T Series Hose Transition to a Crimped Design
Description and Reason for Change: Swagelok's Hose Service Group is transitioning the T series hose from a swaged end connection to a crimped design. The transition will start in Q3 2020 for made-to-stock products, which are listed in the catalog as BHT and MBHT part numbers. The new design offers significant advantages over the older swaged product:
- The new product's performance provides an increase in the pressure rating at elevated temperatures, potentially increasing application uses.
- The transition to crimped components allows us to transition the product from material trace 2 to a trace 1 design with a stamped heat code, improving traceability.
The changes to the product include (see Hose and Flexible Tubing, MS-01-180, for updated technical data):
- Smaller minimum ID and maximum OD due to the crimping dimensions
- Shorter live length due to the extended length of a crimp collar
- Updated appearance of the crimp collar compared to the swaged design
- Improved pressure and temperature ratings
Customers who are purchasing BHT/MBHT products and still require swaged versions in the near future should work with their local Swagelok sales and service center to identify available options.
Effective Date: June 22, 2020
Product Name: Change to Sensor Lock Washer on All ALD3 and ALD6 Valves
Description and Reason for Change: In March 2020, it was announced that the lock washer would no longer be used on select ALD6 assemblies with installed sensors. In the spirit of continuous improvement, we are implementing this change to all ALD3 and ALD6 valve assemblies, excluding ALD3E valves, to improve the consistency of the sensor response. The removal of the lock washer will result in a slight visual change to the assembly.
Effective Date: June 12, 2020
Product Name: Subsea Weld Fitting Dimension Changes to Elbows and Tees
Description and Reason for Change: Due to product improvement efforts, the 1/4 and 3/8 inch subsea weld fitting hex wrench pad and weld tangent length dimensions will be changed, increasing manufacturing efficiency. The overall length and center lines are not affected. This is effective immediately.
These dimensional changes affect the elbow and tee configurations of these sizes only. They will apply to all materials of these sizes and configurations (316L, alloy 2507, and alloy 625).
- Current - 7/16 in. hex wrench pad
- New - 11/16 in. hex wrench pad
Weld Tangent Length:
Current (in) | New (in) |
.75 | .62 |
1.00 | .87 |
1.25 | 1.12 |
1.50 | 1.37 |
2.00 | 1.87 |
The dimensional changes will be reflected in an upcoming revision to the Subsea Weld Fitting catalog, MS-02-481, expected to be released in Q4 2020.
Effective Date: May 4, 2020
Product Name: Swagelok ISO-5211 Compliant Pneumatic Actuator Label Improvement
Description and Reason for Change: We currently offer a variety of ISO-5211 compliant actuators either sold as kits or installed on our general industrial ball valves. To improve the accuracy of the identification on the actuator and provide a clearer understanding of actuator operation, we are implementing changes to the information label printed on each actuator.
Changes to the label include:
- Actuator identifying information grouped together on the left (e.g. serial number, model)
- Technical data grouped together in the upper right (e.g. output torque, temperature range)
- ATEX approval information grouped in the lower right and expanded
- Redundant diagrams removed
The new label will be introduced in the coming months. While this change is implemented, you may see shipments containing both versions of the label until inventory is depleted.
Effective Date: April 30, 2020
Product Name: Change to Finish on EZ Supports
Description and Reason for Change: Effective April 30, 2020, a change to the coating used on EZ Supports will be implemented. All future EZ Supports structural pieces will now have a hot-dipped zinc galvanized finish instead of a zinc metallized finish. The stands, bases, and supports can no longer be provided with the zinc spray metallized finish due to a process change by the supplier.
There is a visual difference between the two finishes. It will not affect fit or function.
Effective Date: March 17, 2020
Product Name: Sensor Lock Washer on Select ALD Valves
Description and Reason for Change: In the spirit of continuous improvement, we are implementing a change to select ALD valve assemblies to improve the consistency of the sensor response. This will result in a slight visual change to the assembly.
Currently a lock washer is present below the jam nut on ALD valves with installed sensors for assembly purposes only; the lock washer does not play a role in the function of the valve assembly. Moving forward, this lock washer will be removed on select assemblies, reducing variability in sensor response times. Please note this does not impact the function of the valve. At this time, this change will only impact the following ordering numbers due to market-specific considerations:
• 6LVV-MSM-ALD6-HF2-P-CS
• 6LVV-MSM-ALD6-HF3-P-CS
While this change is implemented, you may see shipments containing both versions of the valve assembly until the transition is complete. Remaining ordering numbers are currently being evaluated for this change and remain unaffected until further notice.
Effective Date: February 20, 2020
Product Name: Update to 1/4 in. and 6 mm Assembly-by-Torque (AbT) Fittings
Description and Reason for Change: The 1/4 in. and 6 mm sizes of the Assembly-by-Torque (AbT) fitting have been updated to utilize the patented dynamic zone in the nut design to provide a more readily available product and design consistency among all of the AbT fitting sizes. This update complements the prior launch of the 3/8 and 1/2 in., and 8, 10, and 12 mm sizes announced in 2017. All sizes are approved to NGV 3.1, ISO 15500, and ECE-R110.
Effective Date: February 14, 2020
Product Name: Packaging of High-Purity and Ultrahigh-Purity Valves
Description and Reason for Change: Historically, high-purity and ultrahigh-purity valves have been packaged on a white suspension card before being placed into a Swagelok box. Due to the supply chain for white cards, they have been replaced temporarily with brown suspension cards. These brown cards are functionally identical to the white cards with no impact to product quality. Bagging practices and materials will not change.
Effective Date: January 6, 2020
Product Name: Nylon Fittings and Alloy 20 Fittings, Hose and Valves
Description and Reason for Change: Nylon fittings will be discontinued; however, nylon nuts and ferrules will continue to be available.Alloy 20 fitting, hose, and valve products will be discontinued. A selection of valves and fittings in alloy 825, which has material characteristics similar to alloy 20, will continue to be available.
Review 2019 Change notifications
Review 2018 Change notifications
Review Pre-2018 Change notifications
* Applicable changes which would require notification to a Distributor or end user include changes which impact the form, fit or function of a product attribute or measurement as described in Swagelok data readily available to customers or when a change is made that is cosmetically detectable to the customer.
Effective Date: 6/1/17
Description and Reason for Change:
The design for the 2 ounce Snoop bottle has been changed to provide improved seal integrity and an appearance aligned with the 8 ounce bottle, updated in 2016. The plug, tube, and cap will all be the same components used with the 8 ounce bottle. Old style bottles will be used until stock is depleted. The packaging will change accordingly to accommodate the new footprint of the bottle.
Effective Date: 6/1/17
Description and Reason for Change:
The design for the 2 ounce Snoop bottle has been changed to provide improved seal integrity and an appearance aligned with the 8 ounce bottle, updated in 2016. The plug, tube, and cap will all be the same components used with the 8 ounce bottle. Old style bottles will be used until stock is depleted. The packaging will change accordingly to accommodate the new footprint of the bottle.