alert icon

Internet Explorer 8 or 9 is not supported by this website. Please either update your version of Internet Explorer, or use a more up to date browser.

Hide Message hide icon
San Diego | Orange Fluid System Technologies

Your Authorized Swagelok Product and Service Center

A lot of designers automatically select a pipe or tubing when planning out a new fluid system. Working with a known material adds a level of comfort, but there are other factors to consider.

When using a rigid material like pipe, it must be installed either straight or as a series of angels cut to exact lengths. Compound directions involve more exact lengths and numerous connections, and every connection is a potential leak point.  

Hose vs tubing

Hose, on the other hand, perfectly lends itself to bending and routing. Its inherent flexibility means that it will require only end connectors, not one for every directional shift.

And how does having fewer connections benefit the system owner?

  • Material and labor costs are lowered
  • Leakage risk is reduced
  • Chance of pressure drop is minimized
  • Possibility of media being entrapped is lessHose installation

Yet another advantage of hose over rigid materials is that hose can compensate for small discrepancies in distances between connection points, so long as bend radiuses are properly maintained. 

Often in system design tweaks are necessary. Hose can mean less scrap in those situations.

Finally, hose can add to simplicity in cleaning and maintenance. They can easily be removed or replaced, and, when coiled, hoses fit inside sterilization equipment. Rigid materials of any significant length exceed the capabilities of most cleaning equipment tanks.

When designing a fluid system, consider the safety advantages and cost reductions possible from the use of flexible hose.

Hose, on the other hand, perfectly lends itself to bending and routing. Its inherent flexibility means that it will require only end connectors, not one for every directional shift.