alert icon

Internet Explorer 8 or 9 is not supported by this website. Please either update your version of Internet Explorer, or use a more up to date browser.

Hide Message hide icon
San Diego | Orange Fluid System Technologies

Your Authorized Swagelok Product and Service Center

Swagelok PTFE hose does not sacrifice strength to gain flexibility. Unique braiding gives the hose minimal force to bend, especially in tight quarters.

hose guide

One of the great advantages of hose over tubing or pipe is flexibility. But even hose has its limits.  Push it too hard, and it will put extra pressure on the connecting points, and may even collapse. Ordinary hose, that is.

Swagelok has set new standards on flexibility with its X, S, and W series of PTFE hose, while maintaining strength. The secret is in a unique process that bonds a nonmetallic fiber braid to the outside of the hose's extruded smooth-bore PTFE core, and then a layer of stainless steel braid is added to the outside of that allowing for additional flexibility, pressure capabilities, and abrasion resistance.  Other options include a silicone cover and an internal insulation wrap. In fact, it's so flexible, it can be bent into a pretzel, which bodes well for use in tight areas with fewer connections.

Swagelok PTFE hose does not sacrifice strength to gain flexibility. The unique braiding gives the hose a minimum force to bend for ease of installation. Hose that requires less force to bend is easier to install, especially in tight quarters.

Tighter radius and ability to handle offset motion

Polyethylene Core Hose Fiber Braid ReinforcementThe flexibility means that Swagelok PTFE hose does not have the kink problems of ordinary PTFE tubing or hose. It can handle a tighter radius. It is also more easily able to handle offset motion. The braiding acts much like a sleeve does when you bend a tube, keeping it from going oval and then flattening. That's called "hoop strength," which also means greater resistance to collapsing in tight bends.

True diameters

Another benefit of Swagelok PTFE hose is that you get the true diameter that you ask for. A lot of hose manufacturers make the hose to an outside diameter specification. But you are running your media through the inside. So while the hose may be sold as quarter-inch, the wall thickness robs you of some of that measurement. Depending on the wall thickness, the loss can mean as much as a 30 percent differential in the flow rate. Swagelok makes these series of PTFE hose to the inside diameter. You get the full quarter inch to work with.

S Series Cutaway PTFE Hose Smooth Bore

Static dissipation

Static dissipative core tube versions are available for Swagelok PTFE hose. These conductive versions incorporate extruded core tube of PTFE with an inner surface of carbon, often referred to as smooth-bore, carbon black-filled PTFE core. Any electrostatic charges are conducted to the end connection which are subsequently grounded. Electrostatic build-up is prevented.